Analog Devices Introduces Automotive Industry’s First Wireless Battery Management System for Electric Vehicles
This press release features multimedia. View the full release here: https://www.businesswire.com/news/home/20200909005610/en/

The implementation of ADI’s wBMS eliminates the traditional wired harness, saving up to 90% of the wiring and up to 15% of the volume in the battery pack, as well as improving design flexibility and manufacturability, without compromising range and accuracy over the life of the battery.
ADI’s wBMS includes all integrated circuits, hardware and software for power, battery management, RF communication, and system functions in a single system-level product that supports ASIL-D safety and module-level security building upon ADI’s proven industry leading BMS battery cell measurement technology. By delivering high accuracy for the lifetime of the vehicle, the system enables maximum energy use per cell required for best vehicle range and supports safe and sustainable zero-cobalt battery chemistries, such as lithium iron phosphate (LFP).
“The transition of battery packs from wired to wireless connectivity enables automotive manufacturers to scale their electric vehicle platforms across multiple vehicle models to meet growing consumer demand,” said
Additional system features enable batteries to measure and report their own performance, increasing early failure detection, and enabling optimized battery pack assembly. The data can be monitored remotely throughout the battery lifecycle – from assembly to warehouse and transport through installation, maintenance and into a second-life phase.
“We are pleased to collaborate with ADI to take the wBMS technology to production as part of our ground-breaking Ultium battery platform,” said
To learn more about ADI’s wBMS, please visit: www.analog.com/electrification
(ADI-WEB)
This release may contain forward-looking statements intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, among other things, statements by Messrs. Helfrich and Morgan and other statements regarding the expected opportunities, utilization, benefits, cost savings, product and service offerings and developments relating to our wireless battery management system that are based on current expectations, beliefs, assumptions, estimates, forecasts, and projections about the industry and markets in which the companies operate. The statements contained in this release are not guarantees of future performance, are inherently uncertain, involve certain risks, uncertainties, and assumptions that are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed in such forward-looking statements, and such statements should not be relied upon as representing
View source version on businesswire.com: https://www.businesswire.com/news/home/20200909005610/en/
Media
Public Relations Manager
josh.destefano@analog.com
Source: