Rapid Prototyping Kit Simplifies Wide-Dynamic-Range GSPS Data Converter-to-FPGA Connectivity
Kit contains hardware and software to rapidly move from prototype to production with FPGA platforms including Xilinx® Ultrascale™ and Zynq®
"The AD-FMCDAQ2-EBZ FMC module offers Xilinx customers up to 2 GHz of
usable analog bandwidth with a JESD204B interface for rapidly
prototyping a variety of wideband RF applications that demand the high
DSP performance available in Xilinx UltraScale FPGAs and Zynq All
Programmable SoC devices," said
The AD-FMCDAQ2-EBZ is a prototyping system in an FMC form factor for verifying hardware and processing algorithms and rapidly moving from prototype to production in order to reduce the time and risk associated with designing wideband RF signal processing systems. Its performance, bandwidth and integrated functionality allow designers to achieve better signal acquisition in congested RF environments over a wider bandwidth than ever before with the industry's best dynamic range and noise performance.
The AD-FMCDAQ2-EBZ provides tested reference designs including ultra-high-speed data converters, driver amplifiers, clocks and power management ICs. Also included are HDL (hardware description language) code, device drivers, an eye analyzer tool and online support at ADI's EngineerZone™ online technical support community.
- Learn more about the AD-FMCDAQ2-EBZ Rapid Prototyping Kit and order: www.analog.com/AD-FMCDAQ2-EBZ
-
Download rapid prototyping software:
http://wiki.analog.com/resources/eval/user-guides/ad-fmcdaq2-ebz/hardware/functional_overview
- Download schematics, assembly and build files: http://wiki.analog.com/resources/eval/user-guides/ad-fmcdaq2-ebz/hardware
- Read the AD-FMCDAQ-EBZ User Guide: http://wiki.analog.com/resources/eval/user-guides/ad-fmcdaq2-ebz
- Get questions answered by ADI engineers on EngineerZone™, ADI's online technical support community: http://ez.analog.com/community/fpga
About the AD-FMCDAQ2-EBZ Rapid Prototyping Kit
The AD-FMCDAQ2-EBZ Rapid Prototyping Kit includes an on-board AD9680 dual-channel, 14-bit, 1-GSPS, A/D converter. When converting a 1-GHz input, the A/D converter achieves spurious-free dynamic range (SFDR) performance of 80 dBc and 61.4-dBFS signal-to-noise ratio (SNR) while consuming 1.65 W of total power per channel.
The D/A converter in the kit is the 4-channel, 16-bit, 2.8-GSPS, AD9144, of which two channels are accessed on the board. It features 82-dBc SFDR and a maximum sample rate of 2.8 GSPS, permitting multicarrier generation up to the Nyquist frequency.
The AD9523-1 low-jitter clock generator provides a low-power, multi-output, clock distribution function with low jitter performance, along with an on-chip PLL and VCO with two VCO dividers.
Pricing and Availability
| Product | Availability | Price | ||||||||
|
AD-FMCDAQ2-EBZ |
NOW |
|
About
Innovation, performance, and excellence are the cultural pillars on
which
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe.
Trademarks and registered trademarks are the property of their respective owners.
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20141112005025/en/
EDITORS ONLY CONTACT:
Linda.kincaid@analog.com
or
Porter
Novelli
andrew.maclellan@porternovelli.com
Source:
News Provided by Acquire Media