New Generation of High-Performance Blackfin Processors Optimized for Power-Constrained Industrial Imaging, Audio and Automotive Applications
ADSP-BF70x processor family with up to 800 MMACs performance and 1 MB
of embedded
-
Order samples and rapid development EZ-Kit evaluation boards
http://www.analog.com/BF70xboard -
Download ADSP-BF70x data sheets, reference designs and other technical
documents
http://www.analog.com/BF70x -
Get questions answered by ADI engineers on EngineerZone™,
ADI's online technical processor and DSP support community
http://ez.analog.com/community/dsp
"The ADSP-B70x Blackfin family provides a scalable design approach for
commercial-, industrial- and automotive-grade equipment where systems
engineers must maintain high performance while designing for
environmental regulations, portability, extended battery life and
shrinking power budgets," said
More About the ADSP-B70x Blackfin Processor Family
The ADSP-BF70x Blackfin processors are designed for a range of
industrial and building automation applications, including intelligent
lighting and occupancy sensing and industrial imaging in cameras,
barcode readers and biometric sensors. The processor family's low-power
consumption, new 32-bit math and large on-chip
With software IP protection a growing industry security concern, the
ADSP-B70x Blackfin processor family additionally includes an onboard
crypto hardware accelerator that features fast secure boot with
decryption and authentication. For always-on safety critical
applications, the BF70x series also provides high data integrity with
parity and error-correction code (ECC)-protected memory circuitry. ADI's
new line of highly integrated Blackfin processors is available in single
12 × 12 QFN or 12 × 12 BGA packages starting at under
Blackfin Audio and Video Software Modules Available at No Charge from ADI
For audio and video system architects,
Supported by ADI's CrossCore®
The ADSP-B70x is supported by ADI's award winning Crosscore®
-
Learn more about the
Crosscore Embedded Studio Integrated Development Environment
http://www.analog.com/en/evaluation/adswt-cces/eb.html
The ADSP-BF707 EZ-KIT-Lite development board and new ICE-1000/2000
emulators facilitate the creation, test, and debug of advanced
applications on ADI's latest Processors and DSPs. Working in tandem with
the CrossCore® Embedded Studio development environment, the emulators
provide state-of-the-art support for all JTAG-compliant
Pricing, Evaluation Board and Product Sample Availability
Full-featured 400-MHz, 1-MB SRAM ADSP-BF706 (QFN) and ADSP-BF707 (BGA)
product samples are available today. With multiple memory variants,
pricing for the ADSP-BF70x family starts at
About
Innovation, performance, and excellence are the cultural pillars on
which
Blackfin and CrossCore are registered trademarks and EngineerZone is
a trademark of
To subscribe to ADI's News Feed: http://www.analog.com/en/homepage/news.xml
Follow ADI on Twitter: http://www.twitter.com/ADI_News
Subscribe to Analog Dialogue, ADI's monthly technical journal: http://www.analog.com/library/analogDialogue/
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20140612005013/en/
joe.dussi@analog.com
or
andrew.maclellan@porternovelli.com
Source:
News Provided by Acquire Media