Integrated Analog Front-end Simplifies Sensor Interfaces
The ADA4350 features low-noise performance at low frequencies of 90nV/√Hz at 10 Hz and broadband noise of 5 nV/√Hz at 100 kHz to maximize the signal-to-noise ratio of the sensor output. Wide dynamic range measurement for small, sensitive signals such as photons or electrons is enabled with the inclusion of integrated gain switching. The on-chip programmability of the ADA4350 allows designers to select external, optimized feedback components. With one chip, a single-ended or differential sensor current or voltage signal can be transformed to a high-speed, low-noise, single-ended or differential-output voltage.
- Download data sheet, view product page and order samples: http://www.analog.com/ADA4350
- Order the ADA4350 evaluation board: http://www.analog.com/EVAL-ADA4350
- Get questions answered by ADI engineers on EngineerZone®, ADI's online technical support community: https://ez.analog.com/community/amplifiers
In analytical measurement applications, light may need to be monitored over many decades of intensity. This requires a variety of gain switching networks that often incorporate multiple external amplifiers and analog switches, which increases the potential for system errors. The ADA4350 integrates the switching networks and input amplifier to minimize leakage and allow the switching network to select up to six externally configurable feedback networks. In test and measurement systems, the same high measurement accuracy must be maintained across the gain levels as the user adjusts the input range of the instrument. For measuring a wider dynamic range, the ADA4350 is an ideal choice because of its high-impedance/low-Ib input amplifier and serial port-controlled switch network. The device also reduces PCB footprint while significantly increasing channel count without thermal density restrictions.
ADA4350 FET Input AFE Features
-
Low noise, low input bias current FET input amplifier
- 90nV/√Hz at 10 Hz
- 5nV/√Hz at 100 Hz
-
Integrated gain switching
- Switch leakage ± 1pA typ
-
Integrated analog to digital converter driver
- Differential and single-ended mode
Pricing, Availability and Complementary Components |
||||||||||||
Product |
Production |
Price Each In |
Packaging | |||||||||
ADA4350 | NOW |
|
28-lead TSSOP | |||||||||
Complementary components for the ADA4350 include the AD7960 PULSAR® differential ADC, ADR4540 voltage reference, and ADP7118 and ADP7182 linear regulators.
About
Follow ADI on Twitter at http://www.twitter.com/ADI_News
Subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/library/analogDialogue/
EngineerZone is a registered trademark of
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20150512005001/en/
grainne.murphy@analog.com
or
Porter
Novelli
andrew.maclellan@porternovelli.com
Source:
News Provided by Acquire Media