Industry's Widest Bandwidth RF Transceiver Speeds Development of 2G-5G Base Stations and Phased Array Radar
This press release features multimedia. View the full release here: https://www.businesswire.com/news/home/20180611005644/en/
Industry's
The ADRV9009 is the industry's first RF transceiver to support all existing cellular standards. The device is tunable over a range of 75 MHz to 6 GHz to support 2G/3G/4G/5G services, which allows cellular equipment manufacturers to adopt a single, compact radio design across all band and power variants. This reduces product design times by as much as half while simplifying the deployment and maintenance of multi-band, multi-standard communications equipment.
"For the first time, designers of cellular communications equipment have
a common radio platform that can handle emerging wideband applications
like 5G while delivering the high performance required by existing 2G,
3G, and 4G applications," said
- View the ADRV9009 RF transceiver product page, download data sheet, order samples and evaluation boards: http://www.analog.com/ADRV9009
- Learn more about the RadioVerse technology and design ecosystem including ADI's RF transceiver product series: http://www.analog.com/RadioVerse
- Watch a video about the RadioVerse ADRV9009 RF transceiver: http://www.analog.com/en/education/education-library/videos/5791529393001.html
Because of its wide bandwidth, low power and small form factor, the ADRV9009 allows designers to meet the escalating radio-channel-count requirements of 5G massive MIMO equipment. The new RF transceiver is a single-chip TDD solution that can also be used in the design of portable, laboratory grade 5G test and measurement devices which are required for field testing of cellular and Internet of Things networks.
For aerospace and defense systems, the ADRV9009 addresses the high-performance requirements of both wideband and narrowband applications such as military communications and signal intelligence. The new RF transceiver platform also features fast frequency hopping for enhanced link security and spectrum efficiency.
For both advanced cellular and phased array radar systems, the ADRV9009 simplifies digital beamforming design by handling local oscillator (LO) synchronization on-chip, eliminating the need for external LOs.
RadioVerse Design and
The RadioVerse™ design and technology ecosystem
accelerates advanced radio design and development and includes market
leading integrated radio platforms, software tools, evaluation and
prototyping platforms, a range of reference designs, and full radio
solutions. To accelerate customers' time to market with the ADRV9009 RF
transceiver, the RadioVerse ecosystem provides a JESD204B FPGA
integration framework, a production-ready RF system-on-module (RF-SoM)
with dual ADRV9009 devices, and a global partnership network to provide
customers additional design and technical services.
|
Pricing and Availability |
||||||||||||
| Part Number |
Sample |
Production |
Price Each in |
Package | ||||||||
|
ADRV9009
Integrated Dual RF Transmitter, Receiver, Observation Receiver |
Now | Now |
|
12 x 12 BGA | ||||||||
|
ADRV9008-1
Integrated Dual RF Receiver |
|
|
|
12 x 12 BGA | ||||||||
|
ADRV9008-2
Integrated Dual Transmitter with Observation Receiver |
|
|
|
12 x 12 BGA | ||||||||
| ADRV9009-W/PCBZ | Now | Now |
|
ADRV9009 Evaluation Kit | ||||||||
| ADRV9008-1W/PCBZ |
|
|
|
ADRV9008-1 Evaluation Kit | ||||||||
| ADRV9008-2W/PCBZ |
|
|
|
ADRV9008-2 Evaluation Kit | ||||||||
About
(ADI-WEB)
RadioVerse is a trademark of
Follow ADI on Twitter at http://www.twitter.com.
Subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/library/analogDialogue/.
View source version on businesswire.com: https://www.businesswire.com/news/home/20180611005644/en/
linda.kincaid@analog.com
Source:
News Provided by Acquire Media