Analog Devices' Ultralow Power Accelerometer Enables Remote IoT Edge Nodes to Monitor Asset Health
This Smart News Release features multimedia. View the full release here: http://www.businesswire.com/news/home/20170314005114/en/
-
View product page, download data sheet, order samples and evaluation
boards:
http://www.analog.com/ADXL372 -
Learn about
Analog Devices' role in providing critical components, tools, and development tools for high-performance IoT applications:
http://www.analog.com/internet-of-things
- Connect with engineers and ADI product experts on EngineerZone®, an online technical support community: https://ez.analog.com/welcome
- Watch a video about the new ADXL372 MEMS accelerometer: http://www.analog.com/ADXL372/Video
Unlike comparable sensors, this ultralow power MEMS sensor has an "instant on" feature and can wake up immediately to acquire the entire waveform, which significantly reduces standby power drain. The resulting low current requirement of less than two microamps while waiting for an impact typically yields years of operation from a single small battery when the sensor is used in a motion-activated system. By using the ADXL372 MEMS accelerometer as part of a remote edge-node device in an IoT application, transient events can be captured and categorized by a localized processor beforehand by being sent to the cloud or other data center via a wireless link. Keeping the analysis localized saves power, time, and prevents unnecessary transfer of data for an event that is actually insignificant.
The wide bandwidth of 3200 Hz and dynamic range of ±200 g make it an excellent fit for a diverse set of asset health-monitoring applications including monitoring of concussions for indication of Traumatic Brain Injury in both athletes and military personnel.
The ADXL372, specified over the -40C to 105 ⁰C range, joins the industry-leading ultralow power, low g ADXL362 MEMS accelerometer as part of ADI's broader ultralow power portfolio of sensors. Both the ADXL372 and ADXL362 accelerometers interface seamlessly with the ultralow power ADuCM4050 microcontroller, which was recently added to the series of IoT-optimized microcontrollers. Other leading-edge microcontrollers include the ADuCM3027 and ADuCM3029; all of these devices feature both active and hibernate modes with ultralow power demands, and target applications where power consumption, security, and robustness are key requirements.
Pricing and Availability
|
Product |
Output |
Full |
Price Each |
Packaging |
||||||||||||
| ADXL372 | Digital | Now |
|
3×3 mm, 16-lead LGA |
About
EngineerZone is a registered trademark of
Subscribe to Analog Dialogue, ADI's monthly technical journal, at:
http://www.analog.com/analog-dialogue.html
Follow ADI on Twitter at http://www.twitter.com/ADI_News
View source version on businesswire.com: http://www.businesswire.com/news/home/20170314005114/en/
linda.kincaid@analog.com
Source:
News Provided by Acquire Media