Analog Devices' Rx/Tx Converters Enable More Reliable Mobile Infrastructure for High-Quality Phone Service
This Smart News Release features multimedia. View the full release here: http://www.businesswire.com/news/home/20160921005011/en/
- View product pages, download data sheets, order samples and evaluation boards: http://www.analog.com/HMC8100 or http:www.analog.com/HMC8200
- Connect with engineers and experts on EngineerZone®, an online technical support community: https://ez.analog.com/community/rf
The HMC8100 IF receiver chip converts RF input signals ranging from 800 MHz to 4,000 MHz down to a single-ended IF signal of 140 MHz at its output. The device includes two voltage gain amplifiers, three power detectors, a programmable automatic gain control block, and select integrated bandpass filters with 14 MHz, 28 MHz, 56 MHz, and 112 MHz bandwidth. The HMC8100 supports all standard microwave frequency bands from 6 to 42 GHz.
The HMC8200 IF transmitter chip converts the industry standard 300 MHz to 400 MHz IF input signal to an 800 MHz to 4000 MHz single-ended RF signal at its output. With IF input power ranges from −31 dBm to +4 dBm, the HMC8200 provides 35 dB of digital gain control in 1 dB steps while an analog voltage gain amplifier continuously controls the transmitter output power from -20 dBm to +5 dBm. The device also features three integrated power detectors.
Pricing and Availability |
||||||||
Product | Sample Availability | Full Production | Price Each per 1,000 | Packaging | ||||
HMC8100LP6JE | Now | Now |
|
40-lead 6 mm x 6 mm LFCSP | ||||
HMC8200LP5ME | Now | Now |
|
32-lead 5 mm x 5mm KFCSP |
About
EngineerZone is a registered trademark of
Follow ADI on Twitter at http://www.twitter.com
Read and subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/library/analogDialogue/
View source version on businesswire.com: http://www.businesswire.com/news/home/20160921005011/en/
linda.kincaid@analog.com
Source:
News Provided by Acquire Media