Analog Devices Introduces New Family of Digital Isolator Devices Optimized for SPI Communications Applications
Based on ADI's award winning iCoupler® digital isolator technology, the ADuM315x SPIsolator™ family delivers six times the clock speed at as little as 1/5th the area and cost of competing optocoupler and digital isolator solutions.
Supporting up to 40-MHz SPI clock speeds, the new digital isolators are over six times faster, over 80 percent smaller and cost as much as 85 percent less than competing optocoupler- or digital isolator-based solutions. Faster SPI clock speeds enable higher throughout in data acquisition systems, allowing for higher performance and more rapid system response times. A high level of functional integration provides system designers with a simple solution for isolating high-speed SPI signals along with commonly required low-speed status and control signals in a single package.
The ADuM315x family supports a range of high-data-rate, SPI communications applications including distributed control systems, programmable logic controllers, and sensor monitors used in industrial automation, instrumentation equipment and motor controls. Watch a video of the ADuM315x SPIsolator family: http://www.analog.com/SPIsolatorVideo.
- Download data sheet, user guide or order samples:
- Mouser and DigiKey are stocking evaluation boards.
- Connect with ADI engineers on EngineerZone™, an online Interface and Isolation technical support community: http://ez.analog.com/community/interface-isolation
More About the ADuM315x SPIsolator Family
The highly integrated ADuM315x SPI digital isolator family simplifies the design of a complete SPI digital isolation solution by using just three components, compared to the 18 to 32 components required by alternative digital isolator- or optocoupler-based solutions. The ADuM315x family features low propagation delay and jitter in the CLK, MO-SI, MI-SO and SS channels to support SPI clock rates of up to 40 MHz. The new digital isolators also support the maximum sample rate for select ADI 12-, 16- and 18-bit precision A/D converters. The family has a 3.75 kVrms isolation rating and will be followed later in 2014 by SPIsolator devices rated to 5 kVrms.
- The ADuM3150 supports a delayed clock output on the master side of the part that can be used with an additional general-purpose port on the master to support up to 40-MHz clock speeds.
- The ADuM3151, ADuM3152 and ADuM3153 provide four high-speed channels and three additional independent, low-data-rate channels in different configurations.
- The ADuM3154 digital isolator provides a slave-select multiplexing system that allows up to four slave devices to be serviced from one isolator.
Pricing and Availability
| Product |
Sample |
Price Each |
Package | ||||||
| July |
|
20-lead SSOP | |||||||
| July |
|
20-lead SSOP | |||||||
| July |
|
20-lead SSOP | |||||||
| July |
|
20-lead SSOP | |||||||
| July |
|
20-lead SSOP | |||||||
| July |
|
20-lead SSOP | |||||||
| July |
|
20-lead SSOP | |||||||
| July |
|
20-lead SSOP | |||||||
| July |
|
20-lead SSOP | |||||||
| July |
|
20-lead SSOP | |||||||
| Product | Availability | Price Each | Package | ||||||
| Now |
|
Evaluation Board | |||||||
| Now |
|
Evaluation Board | |||||||
| Now |
|
Evaluation Board |
About
Innovation, performance, and excellence are the cultural pillars on
which
iCoupler is a registered trademark, and SPIsolator and EngineerZone
are trademarks of
To subscribe to ADI's News Feed: http://www.analog.com/en/homepage/news.xml
Follow ADI on Twitter: http://www.twitter.com/ADI_News
Subscribe to Analog Dialogue, ADI's monthly technical journal: http://www.analog.com/library/analogDialogue/
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20140624005076/en/
joe.dussi@analog.com
or
andrew.maclellan@porternovelli.com
Source:
News Provided by Acquire Media