Press Releases

Analog Devices Introduces Industry's Smallest Isolated DC-to-DC Converters

November 13, 2012 at 4:00 AM EST

New isolated DC-to-DC converters incorporate ADI's isoPower® power isolation technology, shrinking board space by 75 percent compared to competing solutions.

NORWOOD, Mass.--(BUSINESS WIRE)-- Analog Devices, Inc. (ADI), a global leader in high-performance semiconductors for signal-processing applications and a pioneer in digital isolator technology, today introduced the industry's smallest isolated DC-to-DC converters. The ADuM5010, ADuM6010, ADuM521x and ADuM621x use ADI's proprietary isoPower® isolated DC-to-DC converter technology to deliver 150 mW of output power while using less board space than competing module-based solutions. The ADuM521x and ADuM621x also integrate two channels of ADI's award winning iCoupler® data isolation technology to reduce board space by up to 75 percent compared to optocoupler-based alternatives. The converters expand ADI's isolated power portfolio by providing designers with a compact, easy-to-implement, cost-effective approach to meeting both isolated power and data requirements. The combination of size and output power also addresses the growing space and power constraints engineers must consider when designing control systems, test and measurement equipment, power supplies, motor drives, and other industrial and instrumentation applications.

"This new line of isoPower DC-to-DC converters delivers an excellent balance between power and size that will allow customers to design more functionality and efficiency into smaller form factors while continuing to minimize system cost," said David Krakauer, product line manager, iCoupler Digital Isolator Products, Analog Devices. "ADI's collaborative approach, design support and system-level knowledge help our customers take full advantage of our power isolation technology."

All of the new DC-to-DC converters provide regulated, isolated power, adjustable between 3.15 V and 5.25 V. The ADuM5010 and ADuM521x are certified for 2.5-kV rms (1-minute) isolation, while the ADuM6010 and ADuM621x are certified for 3.75-kV rms (1-minute) isolation with further certification for reinforced insulation per VDE 0884-10. By incorporating ADI's iCoupler digital isolator technology, the ADuM521x and ADuM621x reduce component count and simplify and improve design speed, reliability, and efficiency by eliminating the need for optocouplers. Quad-channel versions of these products using ADI's smaller, lower cost isoPower technology are forthcoming.

Isolated DC-to-DC Converters Reduce System Development Time

Analog Devices pre-certifies its converter modules to help designers reduce system development time, unlike multi-component discrete DC-to-DC converters, which require that designers undertake the costly and time consuming process of individually certifying a dozen or more parts. Additionally, ADI's isolated DC-to-DC converter modules require no added components aside from two bypass capacitors, easing design complexity and reducing time to market.

ADuM5010/ADuM6010 and ADuM521x/ADuM621x Isolated DC-to-DC Converter Key Features

  • Small package: 20-lead SSOP with 5-mm creepage
  • Regulated 3.15-V or 5.25-V output
  • Up to 150-mW output power
  • High speed: 100 Mbps
  • High-temperature operation: 105˚C
  • High common-mode transient immunity: &#62 25-kV/µs

Availability and Pricing

Catalog distributors Digi-Key Corp. and Premier Farnell plc are stocking inventory of both silicon and evaluation boards.

Product    

Sample
Availability

   

2-Channel
iCoupler
Digital Isolation
Core

   

Price per

1k units

    Packaging
ADuM5010     Now     -     $1.54     20-lead SSOP
ADuM6010     Now     -     $2.24     20-lead SSOP
ADuM5210     Now     Yes     $2.32     20-lead SSOP
ADuM5211     Now     Yes     $2.32     20-lead SSOP
ADuM5212     Now     Yes     $3.32     20-lead SSOP
ADuM6210     Now     Yes     $3.36     20-lead SSOP
ADuM6211     Now     Yes     $3.36     20-lead SSOP
ADuM6212     Now     Yes     $3.36     20-lead SSOP
EVAL-ADUM5010EBZ

Evaluation Board

    Now           $59.00 each     -
EVAL-ADUM5210EBZ

2 channel Evaluation Board

    Now           $69.00 each     -

About Analog Devices

Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Celebrating over 40 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.

Follow ADI on Twitter at http://www.twitter.com/ADI_News.

To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe.

iCoupler and isoPower are registered trademarks of Analog Devices, Inc. All other trademarks are the property of their respective owners.

Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=50473171&lang=en

Analog Devices Inc.
Joe Dussi, 781-937-1216
joe.dussi@analog.com
or
Porter Novelli
Andrew MacLellan, 617-897-8270
andrew.maclellan@porternovelli.com

Source: Analog Devices, Inc.

News Provided by Acquire Media