Analog Devices Introduces the Industry's Lowest Power Digital Isolators
The ADuM144x family of iCoupler® digital isolators reduces power by a factor of 1,000 compared to optocouplers to improve energy efficiency and comes in the industry's smallest package
- Order ADuM144x samples, download data sheets and other technical documents by visiting: http://www.analog.com/ADuM144x
- Get digital isolator related questions answered by ADI engineers on EngineerZone™, ADI's online technical support community http://ez.analog.com/community/interface-isolation
-
Catalog Distributors
Digi-Key Corp andMouser Electronics are stocking inventory of both silicon and evaluation boards.
The ADuM144x are quad-channel data isolators available in three different channel configurations with a one-minute isolation safety rating of 2.5 kV rms. They have an operating voltage range of 2.25 V to 3.6 V, further reducing power constraints and providing the lowest isolator operating voltage on the market. Quiescent power supply current at 2.5 V is less than 5 μA per channel, and power supply current at 2 Mbps is less than 380 μA per channel. A power saving mode can reduce current levels to as little as 0.1 μA per channel, resulting in an industry-best 1 μW of total power for the entire isolator. In addition to the significant power savings, the ADuM144x is also available in a 16-lead QSOP package, making it the industry's smallest quad-channel digital isolators with a 2.5 kV rms isolation rating.
"The ADuM144x is a natural extension of our iCoupler digital
isolator product family which includes the highest performance, most
reliable isolators on the market. With the industry's increased focus on
energy efficiency, we recognized that our core iCoupler
technology was the only isolation technology on the market capable of
achieving such low power levels. We worked with customers to define this
breakthrough product family and enhance our capabilities to serve their
system needs," said
The ADuM144x family employs the same iCoupler chip-scale transformer technology used in ADI's full line of safety isolation products and used in the more than one billion channels of isolation shipped in over ten years. The ADuM144x in the 16-lead QSOP package is in production and available today with versions in different packages, channel counts and higher isolation ratings forthcoming.
Pricing and Availability
Product | Availability |
Price
(1K units) |
Package | |||||||||
ADuM144xARQZ | Now |
|
4 mm x 5 mm, 16-lead QSOP | |||||||||
ADuM144xARSZ |
|
|
7.2 mm x 5.3 mm, 20-lead SSOP | |||||||||
Eval Board | Now |
|
||||||||||
About
Innovation, performance, and excellence are the cultural pillars on
which
Follow ADI on Twitter at http://www.twitter.com/ADI_News
To subscribe to ADI's News Feed: http://www.analog.com/en/homepage/news.html
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/library/analogDialogue/
iCoupler® is a registered trademark of
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20131113005053/en/
joe.dussi@analog.com
or
andrew.maclellan@porternovelli.com
Source:
News Provided by Acquire Media