Analog Devices' Data Acquisition IC Simplifies Industrial and Instrumentation Equipment Design
ADI's ADAS3022 integrates a complete precision data acquisition analog signal chain in a single integrated circuit.
- Download data sheet, view product page, and request samples: http://www.analog.com/ADAS3022
- Get support at ADI's EngineerZone™ online technical support community: http://ez.analog.com/welcome
"With a dominant global data conversion market share of approximately
48.5 percent in 2011,
The ADAS3022 data acquisition IC integrates ADI's 16-bit PulSAR® successive-approximation A/D converter core with high-impedance input buffers and a 7-stage on-chip PGIA (programmable-gain instrumentation amplifier). The ADAS3022 includes an 8-channel, low-leakage multiplexer and precision low-drift 4.096-V reference. With eight data channels and delivering full 16-bit dynamic range, the new IC is optimized to interface with a wide range of sensors running from ±10 V to as low as ±640 mV.
The ADAS3022 offers a complete factory calibrated and tested signal chain. This addresses the settling time, signal buffering, level shifting, noise amplification/rejection and other analog signal-conditioning challenges that were once a standard part of the system design process.
Recommended Complementary Components
Complementary components for the ADAS3022 include the ADR381
band gap voltage reference, ADR434x
XFET voltage reference, ADR454x
ultra-low-noise voltage reference,
Pricing and Availability
| Product | Sampling |
|
Price Each Per 1,000 | Packaging | ||||||||||||
| Now | —40°C to +85°C |
|
6 mm x 6 mm
40-lead LFCSP ((lead-frame chip-scale package) |
|||||||||||||
About
Innovation, performance, and excellence are the cultural pillars on
which
*
Follow ADI on Twitter at http://www.twitter.com/ADI_News
Subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/library/analogDialogue/
PulSAR is a registered trademark of
Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=50473242&lang=en
grainne.murphy@analog.com
or
andrew.maclellan@porternovelli.com
Source:
News Provided by Acquire Media