Analog Devices Announces Apollo MxFE Advanced Software-Defined Signal Processing Solution for Aerospace & Defense, Instrumentation, and Next-Generation Wireless Communications
This press release features multimedia. View the full release here: https://www.businesswire.com/news/home/20230613005033/en/

The growth of data intensive applications is increasing the need for wider bandwidths and more rapid processing and analysis of data for 5G, 6G, Wi-Fi 7 & 8, radar, signal intelligence, and other applications at the network edge. As a result, customers need a solution that enables higher-speed data conversion and processing capabilities, while reducing electronic testing complexity.
Developed for application versatility and rapid customization, the Apollo MxFE offers instantaneous bandwidths as high as 10GHz while directly sampling and synthesizing frequencies up to 18GHz (
“The flexibility and simplicity designed into the Apollo MxFE platform have the potential to transform future engineering design for Intelligent Edge devices,” said
Apollo MxFE Product Details
Apollo MxFE’s 4T4R product offers four 12-bit RF ADCs with a sample rate up to 20GSPS, four 16-bit RF DACs with a sample rate up to 28GSPS, an RF input bandwidth from DC to 18GHz (
The on-chip digital signal processing (DSP) offers a real-time FFT Sniffer, a full-rate programmable FIR filter, a 128-tap complex FIR filter, fast-hopping NCOs, DDCs/DUCs, and a fractional sample rate converter. The DSP is dynamically configurable, allowing for rapid changes between narrowband and wideband profiles without taking down the JESD link. Apollo MxFE supports JESD 204B/C and a very short reach (VSR) interface.
Apollo MxFE’s 8T8R product offers eight RF ADCs with a sample rate up to 8GSPS, eight RF DACs with a sample rate up to 16GSPS, an RF input bandwidth up to 16GHz, and an instantaneous bandwidth up to 3GHz. The on-chip DSP offers similar features and functionality to the 4T4R device with double the number of digital blocks, all dynamically configurable.
Apollo MxFE Ecosystem
Apollo MxFE is at the heart of a larger ecosystem of new ADI hardware and software products, each offering complementary capabilities for optimal performance and ease of use. Apollo MxFE is augmented by high-performance variable gain amplifiers, ultralow noise LDO and Silent Switcher® regulators, clocking, and multichip synchronization, along with embedded digital and software technologies including algorithms and security.
The Apollo MxFE ecosystem is comprised of the following products:
- A PLL/VCO synthesizer with a fundamental frequency output of up to 22GHz, extraordinary noise performance, temperature stability (0.06ps/°C), and <1ps alignment resolution.
- A complete, high-performance power solution including the LTM4702 8A µModule regulator. It features Silent Switcher 3 technology, combining an ultralow noise reference with Silent Switcher architecture to achieve high efficiency, excellent wideband noise performance, and maximum overall Apollo MxFE ecosystem performance.
- A 10-channel precision synchronizer for time alignment of SYSREF signals to within 5ps for simultaneous sampling across multiple Apollo MxFE on the same card or across different chassis. It also has the ability to support two-dimensional system synchronization (fanout and/or daisy chain architectures) for very large systems.
- Companion TxVGA and RxVGA solutions provide Apollo MxFE with +15dB of gain and the transition from single-ended to differential on Rx as well as differential to single-ended on Tx. This simplifies the connection to the RF front end.
ADI is demonstrating Apollo MxFE at IMS 2023 (
About
All trademarks and registered trademarks are the property of their respective owners.
(ADI-WEB)
View source version on businesswire.com: https://www.businesswire.com/news/home/20230613005033/en/
Ferda.Millan@analog.com
Source: