Analog Devices and Renesas Electronics Collaborate on 77/79-GHz Automotive RADAR Technology to Improve ADAS Applications and Enable Autonomous Vehicles
New RADAR Sensor Demonstrator Includes RH850/V1R-M Microcontroller from Renesas Autonomy™ Platform and Analog Devices' Drive360™ Advanced 28nm CMOS RADAR Technology
"RADAR sensors play a crucial role for all ADAS or automated driving
functions," said
"Analog Devices' collaboration with Renesas will be a key enabler for
the highest performance RADAR systems," said
About Analog Devices Drive360 28nm CMOS RADAR Technology
Analog
Devices Drive360 28nm CMOS RADAR technology platform builds on the
company's established ADAS, MEMS, and RADAR technology portfolio widely
used throughout the automotive industry for the past 20 years. Drive360
is already revolutionizing sensor performance for ADAS applications with
the world's first automotive RADAR technology based on advanced 28nm
CMOS with unparalleled RF performance for target identification and
classification. ADI's high-performance RADAR solution enables earlier
detection of smaller and faster moving objects. High output power
enables greater range and identification of smaller objects, while
lowest phase noise enables best unambiguous detection of smaller objects
in the presence of large objects.
About the Renesas Autonomy Platform and RH850/V1R-M RADAR MCU
Renesas
is the only automotive semiconductor supplier in the industry to offer
end-to-end solutions from secure cloud connectivity and sensing to
autonomous control. Leveraging decades of experience and technological
expertise, the new Renesas autonomy Platform is an open, innovative, and
trusted platform for ADAS and automated driving, supported by Renesas'
sustainable and scalable SoC and MCU roadmaps. The RH850/V1R-M MCU was
specifically designed for use in RADAR applications as part of the
sustainable and scalable portfolio. The new MCU includes optimized
programmable digital signal processing (DSP), a dual CPU cores each
operating at 320 megahertz (MHz) with industry-leading high speed flash
of 2 megabyte (MB), and 2 MB internal RAM, while meeting the industry's
highest temperature requirements.
About
About
Drive360 is a trademark of
Renesas autonomy is a trademark of
View source version on businesswire.com: http://www.businesswire.com/news/home/20170411005016/en/
linda.kincaid@analog.com
or
kyoko.okamoto.sx@renesas.com
Source:
News Provided by Acquire Media