Analog Devices and Marvell Showcase Next-Generation 5G Massive MIMO Radio Unit Platform at Mobile World Congress 2023
Collaboration combines industry-leading digital beamforming and transceiver silicon to propel advanced massive MIMO into mainstream
This press release features multimedia. View the full release here: https://www.businesswire.com/news/home/20230223005331/en/

“As mMIMO radio functionality grows in complexity, more specialized silicon approaches are required,” said
Together, the RadioVerse Transceiver SoC and the OCTEON 10 Fusion processor support the entire signal chain with unmatched RU system efficiency. The ADRV9040 RadioVerse Transceiver SoC includes substantial digital capabilities including linearization algorithms for boosting power amplifier efficiency and performance, as well as digital channel filters which reduce interface rates. The OCTEON 10 Fusion 5G baseband processor has specialized accelerators optimized for efficiently processing complex beamforming algorithms, along with dedicated processors for the low PHY baseband which can be configured for the various O-RAN split 7.2x configurations.
“Infrastructure vendors face many challenges when developing O-RAN mMIMO radio units, including access to optimized semiconductors,” said
“Marvell is pleased to collaborate with ADI in taking mMIMO radios to the next level,” said
The reference design, which is expandable to support a 64T64R configuration, supports 32 transmit and receive antennas (32T32R) with 400 MHz of operational bandwidth and 300 MHz of instantaneous bandwidth. The OCTEON 10 Fusion 5G baseband processor and RadioVerse SoC leverage hardware accelerators as well as the industry-leading RF and digital baseband process nodes shipping commercially—16 nm and 5 nm respectively—delivering up to 40% reduction in energy consumption per bit as compared over the previous generation. The platform enables Network Energy Savings (NES) modes, which deliver additional power savings.
The platform is on display at
About
About
To deliver the data infrastructure technology that connects the world, we’re building solutions on the most powerful foundation: our partnerships with our customers. Trusted by the world’s leading technology companies for over 25 years, we move, store, process and secure the world’s data with semiconductor solutions designed for our customers’ current needs and future ambitions. Through a process of deep collaboration and transparency, we’re ultimately changing the way tomorrow’s enterprise, cloud, automotive, and carrier architectures transform—for the better.
Disclaimer: This press release contains forward-looking statements within the meaning of the federal securities laws that involve risks and uncertainties. Forward-looking statements include, without limitation, any statement that may predict, forecast, indicate or imply future events, solutions, or achievements. Actual events or results may differ materially from those contemplated in this press release. Forward-looking statements speak only as of the date they are made. Readers are cautioned not to put undue reliance on forward-looking statements, and no person assumes any obligation to update or revise any such forward-looking statements, whether as a result of new information, future events or otherwise.
All trademarks and registered trademarks are the property of their respective owners.
View source version on businesswire.com: https://www.businesswire.com/news/home/20230223005331/en/
Ferda.Millan@analog.com
pr@marvell.com
Source: