Analog Devices Unveils Direct Conversion Receiver Development Platform for Radar Systems
AD-FMCOMMS6-EBZ supports key L- and S-band frequency radar bands.
- Learn more and order the AD-FMCOMMS6-EBZ: http://www.analog.com/AD-FMCOMMS6-EBZ
- View the user guide and download the design files: http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms6-ebz/hardware
- Connect with the ADI experts in EngineerZone®, an online technical support community: http://ez.analog.com
The AD-FMCOMMS6-EBZ receiver platform integrates the AD9652 dual 16-bit A/D converter, ADL5566 high-dynamic-range RF/IF dual differential amplifier, and ADL5380 quadrature demodulator, all of which are COTS (commercial-off-the-shelf) components. A complete design support package is available for the AD-FMCOMMS6-EBZ, and includes schematics, layout files, noise analysis worksheet, FPGA HDL (hardware description language) code, and software drivers.
About the AD-FMCOMMS6-EBZ Receiver Development Platform
The
AD-FMCOMMS6-EBZ utilizes an I/Q demodulator to implement a direct
conversion or zero IF architecture in which just one frequency
translation is required, compared to a super-heterodyne receiver that
must perform several frequency translations. A single frequency
translation is advantageous because it reduces receiver complexity and
the number of conversion stages needed, which in turn increases
performance and reduces power consumption. The architecture also avoids
image rejection issues and unwanted mixing by adding an amplification
stage to maintain the full-scale input to the A/D converter. In
addition, the image rejection inherent to the I/Q modulation scheme
removes the need for an expensive anti-aliasing filter. The on-board
local oscillator and converter clock share the same reference signal to
prevent smearing.
The AD-FMCOMMS6-EBZ receiver development platform incorporates a full direct-receive signal chain path and has a bandwidth of 220 MHz with a pass-band flatness of +/- 1.0 dB. The RF input range of the ADL5380 demodulator is 400 MHz to 6 GHz and is powered by a single 5-V supply. The ADL5566 4.5-GHz dual differential amplifier is optimized for IF and dc applications and provides a gain of 16 dB. The AD9652 dual 16-bit, 310-MSPS A/D converter achieves the industry's lowest noise at the highest speed; this level of performance enables target identification at a much longer range. The SNR and SFDR measured at an IF of 145 MHz are 64 dB and 78 dBc, respectively. Additional on-board functionality includes power management and clock distribution with fanout.
Pricing and Availability |
|||||||||
Part Number | Availability | Unit Price | Package | ||||||
NOW |
|
FMC | |||||||
About
Innovation, performance, and excellence
are the cultural pillars on which
EngineerZone is a registered trademark of
Follow ADI on Twitter at http://www.twitter.com/ADI_News
Subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/library/analogDialogue/
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20141210005008/en/
Linda.kincaid@analog.com
or
Porter
Novelli
andrew.maclellan@porternovelli.com
Source:
News Provided by Acquire Media