First Synchronized RF Transceiver Rapid Prototyping Kit for SDR Launched
Features Analog Devices's award-winning dual AD9361 RF Transceiver ICs; new SDR design resources for multi-channel synchronization and system simulation
The AD-FMCOMMS5-EBZ rapid prototyping kit includes: an FPGA mezzanine card (FMC) featuring two of Analog Devices' award-winning AD9361 2 x 2 RF Transceivers and support circuitry, reference designs, design and simulation tools for MathWorks, HDL (hardware description language) code, device drivers for Zynq-7000 All Programmable SoCs and online support at ADI's EngineerZone for rapid prototyping to reduce development time and risk.
View this video about Analog Device's rapid prototyping kits: http://videos.analog.com/video/products/rf-ics/3701552681001/Synchronized-RF-Transceiver-Rapid-Prototyping-Kit-for-SDR/
- To learn more and order the AD-FMCOMMS5-EBZ: www.analog.com/ad-FMCOMMS5-EBZ
- To learn more about ADI's SDR portfolio: www.analog.com/sdr
- Connect with engineers and SDR experts on EngineerZone™, an online technical support community: https://ez.analog.com/community/wide-band-rf-transceivers
The AD-FMCOMMS5-EBZ rapid prototyping kit is the fifth SDR rapid
prototyping kit ADI has introduced in the last year to help customers
address the global SDR market that is expected to double to
About The AD9361 RF Transceiver
The AD9361 operates over a frequency range of 70 MHz to 6 GHz. It is a complete radio design that combines multiple functions, including an RF front end, mixed-signal baseband section, frequency synthesizers, two analog-to-digital converters and two direct conversion receivers in a single chip. The AD9361 supports channel bandwidth from less than 200 kHz to 56 MHz, and is highly programmable, offering the widest dynamic range available in the market today with state-of-the-art noise figure and linearity.
Design and Simulation Tools for ADI RF Transceivers
SimRF™ by MathWorks provides a simulation engine for designing RF systems and includes models of the AD9361 and AD9364 for a seamless transition from software simulation to hardware in the loop. In addition, the FIR Filter Design MATLAB® application can be used to select and design digital filters for the AD9361 with minimum trial and error, create custom filters, and examine filter performance. The output can be exported into a SimRF model or hardware. ADI offers a comprehensive suite of RF design tools including ADIsimRF™, ADIsimPLL™, and ADIsimCLK™.
Pricing and Availability |
|||||||||||||||
Part Number | Availability | Unit Price | Package | ||||||||||||
NOW |
|
FMC | |||||||||||||
About
Innovation, performance, and excellence are the cultural pillars on
which
Follow ADI on Twitter at http://www.twitter.com/ADI_News
Subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/library/analogDialogue/
* Forecast Analysis to 2014-2020
(Defense, Commercial & Homeland
Security)
SOFTWARE DEFINED RADIOS MARKET
MarketsandMarkets.com
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20140805005133/en/
Bob.olson@analog.com
or
andrew.maclellan@porternovelli.com
Source:
News Provided by Acquire Media