Press Releases

Analog Devices' MEMS Accelerometers Deliver Compelling Noise Performance for Condition Monitoring Applications

April 24, 2017 at 8:00 AM EDT

NORWOOD, Mass.--(BUSINESS WIRE)-- Analog Devices, Inc. (ADI) today announced two high frequency, low noise MEMS accelerometers designed specifically for industrial condition monitoring applications. The ADXL1001 and ADXL1002 MEMS accelerometers deliver the high resolution vibration measurements necessary for early detection of bearing faults and other common causes of machine failure. Historically, inadequate noise performance of available high frequency MEMS accelerometers compared with legacy technology held back adoption, failing to take advantage of MEMS reliability, quality and repeatability. Today, the ADXL1001 and ADXL1002 noise performance over high frequencies is on par with available PZT technology, and make ADI MEMS accelerometers a compelling option for new condition monitoring products. The ADXL1001 and ADXL1002 are the latest examples of high performance precision sensing technology from Analog Devices, providing high quality and accurate data for Smart Factory Internet of Things applications, and enabling intelligent sensing from the edge of the network.

This Smart News Release features multimedia. View the full release here: http://www.businesswire.com/news/home/20170424005014/en/

Analog Devices' MEMS Accelerometers Deliver Compelling Noise Performance for Condition Monitoring Ap ...

Analog Devices' MEMS Accelerometers Deliver Compelling Noise Performance for Condition Monitoring Applications (Photo: Business Wire)

About the ADXL1001 and ADXL1002
The ADXL1001 and ADXL1002 MEMS accelerometers deliver ultra-low noise density over an extended bandwidth with high-g range. The accelerometers are available in two models with full-scale ranges of ±100g (ADXL1001) and ±50g (ADXL1002). Typical noise density for the ADXL1002 is 25 μg/√Hz, with a sensitivity of 40mV/g, and 30 μg/√Hz for ADXL1001 with sensitivity 20mV/g. Both accelerometers operate on single voltage supply from 3.0V to 5.25V, and offer useful features such as complete, electrostatic self-test and over range indicator. The ADXL1001 and ADXL1002 are rated for operation over a -40°C to +125°C temperature range.

 

Product Pricing and Availability Product Pricing and Availability

Product    

Output
Interface

   

Full-scale
Range

   

Product
Availability

   

Price Each
per 1,000

    Packaging
ADXL1001     Analog     ±100 g     Now     $29.61    

32 lead 5x5 mm
LFCSP

ADXL1002     Analog     ±50 g     Now     $29.61    

32 lead 5x5 mm
LFCSP

                   

About Analog Devices
Analog Devices is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com

EngineerZone is a registered trademark of Analog Devices, Inc.
Follow ADI on Twitter at http://www.twitter.com/ADI_News
Read and subscribe to Analog Dialogue, http://www.analog.com/analog-dialogue.html

Analog Devices, Inc.
Linda Kincaid
linda.kincaid@analog.com

Source: Analog Devices, Inc.

News Provided by Acquire Media